pins state during POR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pins state during POR

Jump to solution
1,949 Views
eishishibusawa
Contributor III

Dear Sir

 

I want to ask you about i.MX6ULL.

 

Q1.

I want to know the state of the pins during POR is asserted.

Does it have been described in the manual or data sheet?

 

Best Regards,

Eishi SHIBUSAWA

Labels (1)
0 Kudos
Reply
1 Solution
1,815 Views
Yuri
NXP Employee
NXP Employee

Hello,

  There are pin states, provided in the DataSheet(s), relate to situation just after reset ;

pin states during power on \ reset are not guaranteed.

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
2 Replies
1,816 Views
Yuri
NXP Employee
NXP Employee

Hello,

  There are pin states, provided in the DataSheet(s), relate to situation just after reset ;

pin states during power on \ reset are not guaranteed.

Regards,

Yuri.

0 Kudos
Reply
1,815 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the data sheet:

"The SRC_POR_B signal controls the processor POR and must be immediately asserted at
power-up and remain asserted until the VDD_ARM_CAP, VDD_SOC_CAP, and VDD_PU_CAP
supplies are stable. VDD_ARM_IN and VDD_SOC_IN may be applied in either order with no
restrictions."

for more detailed information, pls refer to the Power-Up Sequence of data sheet.

0 Kudos
Reply