pf0100f9azes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pf0100f9azes

2,995件の閲覧回数
hailiu
Contributor IV

I used PF0100F9AZES PMIC to generate system power, one board generate all the correct power, the other one has some issues. According to the spec, Vgen2 pin 18) should generate a 1.5V output, but I get a 2.8V output, sw4LX (pin 21), after the inductor, I should get a 1.8V output, but I get a 2.4V output? some things wrong? or the chip was not programmed correctly?

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,971件の閲覧回数
hailiu
Contributor IV

I guess that because the output of pin 21 (SW4LX) is 2.4V, the input to pin 17 is 2.4V, that's cause the output of Vgen2 is high. I checked the inputs on pin 7,10,12, there are all 4.36V, it seems a reasonable value, the problem is why output of sw4 is high?

0 件の賞賛
返信

2,957件の閲覧回数
hailiu
Contributor IV

Found the problem. Not the pmic problem, but the output pin was shorted to a 3.0v trace.

Thank you very much.

2,972件の閲覧回数
hailiu
Contributor IV

vgen1 (pin 16) are 0V for all three boards.

0 件の賞賛
返信

2,987件の閲覧回数
Yuri
NXP Employee
NXP Employee

@hailiu 
Hello,

 

    Is it possible to look at schematic?

Regards,
Yuri.

 

0 件の賞賛
返信

2,974件の閲覧回数
hailiu
Contributor IV

Hello Yuri,

I assembled three boards, one outpiu voltage is OK except 1.2V, which I don't need it, the other two have the same issue and the voltage are the same, 2.3V and 2.8V, instead of 1.5V  and 1.8V. included is the schemmatics.systemPower.jpg

0 件の賞賛
返信