performance of CAAM on imx8qxp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

performance of CAAM on imx8qxp

1,392件の閲覧回数
shuaiqing_wang
Contributor I

HI NXP team:

We are working on caam hash performance test on i.MX8 board.

It is strange that sha1 performance is lower than sha256's.

As far as i know, the computation of sha256 algorithm is more complicated than sha1,

so I want to know why sha1 hash time is longer than sha256's.

 

I know the hash time is depend on the algorithm implementation.

Following is the test result, please help to confirm if it is normal data of test result?

If you are working on it, please let me know. Or please share the schedule.

 

Hash SHA1: 16 MByte data takes 94 msec.

----------------------------------------------------

Job ring parameters:

g_job->dsc[0]:b0800007
g_job->dsc[1]:8441000d
g_job->dsc[2]:24540000
g_job->dsc[3]:84ef0a40
g_job->dsc[4]:1000000
g_job->dsc[5]:54200014
g_job->dsc[6]:81edef00

-----------------------------------------------------

 

Hash SHA256: 16 MByte data takes 81 msec.

------------------------------------------------------

Job ring parameters:

g_job->dsc[0]:b0800007
g_job->dsc[1]:8443000d
g_job->dsc[2]:24540000
g_job->dsc[3]:84ef0a40
g_job->dsc[4]:1000000
g_job->dsc[5]:54200020
g_job->dsc[6]:81edef00

-----------------------------------------------------

 

Looking forward to you reply.

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,302件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

I’m afraid that i.MX8QXP is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信