patch for NAND Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,950件の閲覧回数
Harris
Contributor III

Is there a patch to resolve NAND Flash driver.

I found the Spansion NAND S34ML08G1 can not be support by IMX6Q.

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
6,619件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Harris

general steps for adding new nand support are as follows

(there may be slight differencies depending on kernel):

add support as describes attached Add new_NAND support.pdf.

Then rebuild MFG Tool firmware (initramfs.cpio.gz.uboot), as

describes sect.3.9 "Build Manufacturing Firmware"

i.MX_6DualQuad_SABRE_AI_Linux_User_Guide.pdf, then

use MFG Tools for programming NAND (or commands

given in profile "MX6Q-Sabreauto-NAND" in ucl2.xml.)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

5 返答(返信)
6,619件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Harris

it is in red colour attachment, please check my previous answer at 28.04.2016 5:38,

then click on red with mouse.

1.jpg

Best regards

igor

0 件の賞賛
返信
6,619件の閲覧回数
Harris
Contributor III

Many Thanks.

0 件の賞賛
返信
6,620件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Harris

general steps for adding new nand support are as follows

(there may be slight differencies depending on kernel):

add support as describes attached Add new_NAND support.pdf.

Then rebuild MFG Tool firmware (initramfs.cpio.gz.uboot), as

describes sect.3.9 "Build Manufacturing Firmware"

i.MX_6DualQuad_SABRE_AI_Linux_User_Guide.pdf, then

use MFG Tools for programming NAND (or commands

given in profile "MX6Q-Sabreauto-NAND" in ucl2.xml.)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

6,619件の閲覧回数
Harris
Contributor III

Would you please give me the new_NAND support.pdf.

Thanks.

0 件の賞賛
返信
6,619件の閲覧回数
Harris
Contributor III

Hi, Igor,

Thank you for your reply.

hwo to get the new_NAND support.pdf?

Thanks.

0 件の賞賛
返信