parallel RGB data enable in imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

parallel RGB data enable in imx6

1,736 Views
redwanmohamed
Contributor III

We have used DI0_PIN4 pad in our design for data enable signal for the parallel RGB interface, which we have configured as below in the dts (but not getting data enable signal as expected)

MX6QDL_PAD_DI0_PIN4__IPU1_DI0_PIN04

I was going through the IMX6DQCEC.pdf which says IPUx_DIx_PIN15 as data enable signal. Please advice whether we can use IPUx_DIx_PIN4 as data enable or not

Labels (4)
0 Kudos
Reply
1 Reply

1,412 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following

https://community.nxp.com/message/339428 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply