parallel RGB data enable in imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

parallel RGB data enable in imx6

1,275 次查看
redwanmohamed
Contributor III

We have used DI0_PIN4 pad in our design for data enable signal for the parallel RGB interface, which we have configured as below in the dts (but not getting data enable signal as expected)

MX6QDL_PAD_DI0_PIN4__IPU1_DI0_PIN04

I was going through the IMX6DQCEC.pdf which says IPUx_DIx_PIN15 as data enable signal. Please advice whether we can use IPUx_DIx_PIN4 as data enable or not

标签 (4)
0 项奖励
回复
1 回复

951 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following

https://community.nxp.com/message/339428 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复