ovdd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ovdd

1,611件の閲覧回数
priyangeorge
Contributor I

Hi all,

     Can anyone please tell me the value of OVDD for GPIO in I.mx 257.

Regards,

Priyan George

ラベル(1)
0 件の賞賛
返信
1 返信

1,491件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Priyan

according to i.MX25 Datasheet (rev.10, 7/2013) sect.3.5 I/O DC Parameters

http://www.freescale.com/files/dsp/doc/data_sheet/IMX25CEC.pdf  :

The term ‘OVDD’ in this section refers to the associated supply rail of an

input or output. The association is shown in the “Signal Multiplexing”

chapter of the reference manual.

Associated supply rail can be found in Table 101. 17×17 mm Package i.MX25

Signal Contact Assignment

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信