ovdd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ovdd

1,580 Views
priyangeorge
Contributor I

Hi all,

     Can anyone please tell me the value of OVDD for GPIO in I.mx 257.

Regards,

Priyan George

Labels (1)
0 Kudos
Reply
1 Reply

1,460 Views
igorpadykov
NXP Employee
NXP Employee

Hi Priyan

according to i.MX25 Datasheet (rev.10, 7/2013) sect.3.5 I/O DC Parameters

http://www.freescale.com/files/dsp/doc/data_sheet/IMX25CEC.pdf  :

The term ‘OVDD’ in this section refers to the associated supply rail of an

input or output. The association is shown in the “Signal Multiplexing”

chapter of the reference manual.

Associated supply rail can be found in Table 101. 17×17 mm Package i.MX25

Signal Contact Assignment

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply