otg port for debugging using eclipse in i.mx6(android)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

otg port for debugging using eclipse in i.mx6(android)

1,597 Views
bandelaprathyus
Contributor II

Hi,

      In i.mx6 Sabre AI Board ported with android 4.4.3, which is the otg (usb) port that can be connected and debugged using eclipse?

0 Kudos
Reply
1 Reply

1,459 Views
igorpadykov
NXP Employee
NXP Employee

Hi bandela

one can look at application note devoting to i.MX6 debugging

AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors

probably one can consider adb over usb

USB Host and Accessory | Android Developers

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply