otg port for debugging using eclipse in i.mx6(android)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

otg port for debugging using eclipse in i.mx6(android)

1,601件の閲覧回数
bandelaprathyus
Contributor II

Hi,

      In i.mx6 Sabre AI Board ported with android 4.4.3, which is the otg (usb) port that can be connected and debugged using eclipse?

0 件の賞賛
返信
1 返信

1,463件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi bandela

one can look at application note devoting to i.MX6 debugging

AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors

probably one can consider adb over usb

USB Host and Accessory | Android Developers

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信