openvpn client

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

openvpn client

2,296件の閲覧回数
mm7
Contributor I

Hello,

we are actually testing a Display with i.Mx 6 processor and Linux operating system, and we want to cross-compile openvpn client from source code (with an existing toolchain) and try to run it on this Display.

Question, which steps are necessary?, and is a new configuration and build of BSP sw needed?

System information

Embedded Linux version : Linux tera-he 4.1.23-3.2_rc0+g3617c73 #1 SMP PREEMPT Thu Mar 5                                                         16:15:19 CET 2020 armv7l GNU/Linux
BSP Version: 3.2_rc0

 

Best Regards

0 件の賞賛
返信
2 返答(返信)

2,277件の閲覧回数
mm7
Contributor I

Thanks, i will try this!

Regards

 

0 件の賞賛
返信

2,284件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello mm7,

You need to have at least L5.10.35 kernel version BSP, and the latest gcc toolchain, this will compile and make your vpn app on MX6.

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Regards