1.
In Eclipse right click project
Debug As -> Debug Configurations -> GDB Hardware Debugging
2.
click Startup tab
uncheck the all items on startup page
add those lines under [Halt] box but do not check [Halt]
add-symbol-file /root/project_board/free_imx/out/matrix_io/uboot/u-boot 0x4FF04000
start debugging and trace code
(ps: in u-boot os keyin [bdinfo] show relocaddr = 0x4FF04000)
3.
file /root/project_board/free_imx/myandroid/bootable/bootloader/uboot-imx/arch/arm/lib/bootm.c
in function boot_jump_linux(bootm_headers_t *images, int flag)
//break at
kernel_entry = (void (*)(int, int, uint))images->ep;
run step to next line
[Expressions] window show kernel_entry is 0x14008000
4.
Press [Terminate] to stop debug
5.
click Startup tab
uncheck the all items on startup page
add those lines under [Halt] box but do not check [Halt]
add-symbol-file /root/project_board/free_imx/out/matrix_io/kernel/arch/arm/boot/compressed/vmlinux 0x14008000
continue to debug and trace code
6.
file /root/project_board/free_imx/myandroid/kernel_imx/arch/arm/boot/compressed/head.S
//break at
__enter_kernel:
mov r0, #0 @ must be 0
ARM( mov pc, r4 ) @ call kernel
[Registers] window show r4 = 0x10008000
7.
Press [Terminate] to stop debug
8.
click Startup tab
uncheck the all items on startup page
add those lines under [Halt] box but do not check [Halt]
add-symbol-file /root/project_board/free_imx/out/matrix_io/kernel/arch/arm/kernel/head.o 0x80008000 -s .head.text 0x10008000
continue to debug and trace code
9.
file /root/project_board/free_imx/myandroid/kernel_imx/arch/arm/kernel/head.S
//break at
ENTRY(stext)
THUMB( adr r9, BSYM(1f) ) @ Kernel is always entered in ARM.
THUMB( bx r9 ) @ If this is a Thumb-2 kernel,
THUMB( .thumb ) @ switch to Thumb now.
THUMB(1: )
#ifdef CONFIG_ARM_VIRT_EXT
bl __hyp_stub_install
#endif
@ ensure svc mode and all interrupts masked
safe_svcmode_maskall r9
//done ~~~
demo:
Picasa Web Albums - Jesse Stone - i.mx6
解決済! 解決策の投稿を見る。
Debugging Skill - How to debug from u-boot to start_kernel
Programming Guide: Openocd debug u-boot to start_kernel on i.mx6
1.
In Eclipse right click project
Debug As -> Debug Configurations -> GDB Hardware Debugging
2.
click Startup tab
uncheck the all items on startup page
add those lines under [Halt] box but do not check [Halt]
add-symbol-file /root/project_board/free_imx/out/matrix_io/uboot/u-boot 0x4FF04000
start debugging and trace code
(ps: in u-boot os keyin [bdinfo] show relocaddr = 0x4FF04000)
3.
file /root/project_board/free_imx/myandroid/bootable/bootloader/uboot-imx/arch/arm/lib/bootm.c
in function boot_jump_linux(bootm_headers_t *images, int flag)
//break at
kernel_entry = (void (*)(int, int, uint))images->ep;
run step to next line
[Expressions] window show kernel_entry is 0x14008000
4.
Press [Terminate] to stop debug
5.
click Startup tab
uncheck the all items on startup page
add those lines under [Halt] box but do not check [Halt]
add-symbol-file /root/project_board/free_imx/out/matrix_io/kernel/arch/arm/boot/compressed/vmlinux 0x14008000
continue to debug and trace code
6.
file /root/project_board/free_imx/myandroid/kernel_imx/arch/arm/boot/compressed/head.S
//break at
__enter_kernel:
mov r0, #0 @ must be 0
ARM( mov pc, r4 ) @ call kernel
[Registers] window show r4 = 0x10008000
7.
Press [Terminate] to stop debug
8.
use command [arm-eabi-nm]
/root/project_board/free_imx/myandroid/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-nm -a /root/project_board/free_imx/out/matrix_io/kernel/vmlinux | grep .text
813db454 t .exit.text
80008000 t .head.text --->need
81385260 t .init.text
800081c0 t .text --->need
80c90344 t .text.head
0x800081c0 change to 0x100081c0 for .text
0x80008000 change to 0x10008000 for .head.text
9.
click Startup tab
uncheck the all items on startup page
add those lines under [Halt] box but do not check [Halt]
add-symbol-file /root/project_board/free_imx/out/matrix_io/kernel/vmlinux 0x100081c0 -s .head.text 0x10008000
continue to debug and trace code
10.
file /root/project_board/free_imx/myandroid/kernel_imx/arch/arm/kernel/head.S
//break at
ENTRY(__turn_mmu_on)
…
…
...
mov pc, r3
[Registers] window show r3 = 0x813852bc
11.
Press [Terminate] to stop debug
12.
click Startup tab
uncheck the all items on startup page
add those lines under [Halt] box but do not check [Halt]
add-symbol-file /root/project_board/free_imx/out/matrix_io/kernel/vmlinux
[Disassembly] windows find 0x813852bc at __mmap_switched of head-common.S
continue to debug and trace code
13.
file /root/project_board/free_imx/myandroid/kernel_imx/arch/arm/kernel/head-common.S
//break at
__mmap_switched:
adr r3, __mmap_switched_data
…
…
…
b start_kernel
//then go to start_kernel(void) of ~...//kernel_imx/init/main.c
Debugging Skill - How to debug from u-boot to start_kernel
Programming Guide: Openocd debug u-boot to start_kernel on i.mx6
1.
In Eclipse right click project
Debug As -> Debug Configurations -> GDB Hardware Debugging
2.
click Startup tab
uncheck the all items on startup page
add those lines under [Halt] box but do not check [Halt]
add-symbol-file /root/project_board/free_imx/out/matrix_io/uboot/u-boot 0x4FF04000
start debugging and trace code
(ps: in u-boot os keyin [bdinfo] show relocaddr = 0x4FF04000)
3.
file /root/project_board/free_imx/myandroid/bootable/bootloader/uboot-imx/arch/arm/lib/bootm.c
in function boot_jump_linux(bootm_headers_t *images, int flag)
//break at
kernel_entry = (void (*)(int, int, uint))images->ep;
run step to next line
[Expressions] window show kernel_entry is 0x14008000
4.
Press [Terminate] to stop debug
5.
click Startup tab
uncheck the all items on startup page
add those lines under [Halt] box but do not check [Halt]
add-symbol-file /root/project_board/free_imx/out/matrix_io/kernel/arch/arm/boot/compressed/vmlinux 0x14008000
continue to debug and trace code
6.
file /root/project_board/free_imx/myandroid/kernel_imx/arch/arm/boot/compressed/head.S
//break at
__enter_kernel:
mov r0, #0 @ must be 0
ARM( mov pc, r4 ) @ call kernel
[Registers] window show r4 = 0x10008000
7.
Press [Terminate] to stop debug
8.
use command [arm-eabi-nm]
/root/project_board/free_imx/myandroid/prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi-nm -a /root/project_board/free_imx/out/matrix_io/kernel/vmlinux | grep .text
813db454 t .exit.text
80008000 t .head.text --->need
81385260 t .init.text
800081c0 t .text --->need
80c90344 t .text.head
0x800081c0 change to 0x100081c0 for .text
0x80008000 change to 0x10008000 for .head.text
9.
click Startup tab
uncheck the all items on startup page
add those lines under [Halt] box but do not check [Halt]
add-symbol-file /root/project_board/free_imx/out/matrix_io/kernel/vmlinux 0x100081c0 -s .head.text 0x10008000
continue to debug and trace code
10.
file /root/project_board/free_imx/myandroid/kernel_imx/arch/arm/kernel/head.S
//break at
ENTRY(__turn_mmu_on)
…
…
...
mov pc, r3
[Registers] window show r3 = 0x813852bc
11.
Press [Terminate] to stop debug
12.
click Startup tab
uncheck the all items on startup page
add those lines under [Halt] box but do not check [Halt]
add-symbol-file /root/project_board/free_imx/out/matrix_io/kernel/vmlinux
[Disassembly] windows find 0x813852bc at __mmap_switched of head-common.S
continue to debug and trace code
13.
file /root/project_board/free_imx/myandroid/kernel_imx/arch/arm/kernel/head-common.S
//break at
__mmap_switched:
adr r3, __mmap_switched_data
…
…
…
b start_kernel
//then go to start_kernel(void) of ~...//kernel_imx/init/main.c