oneiric problem with login in

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

oneiric problem with login in

2,965件の閲覧回数
thouswave
Contributor III

According to i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf, I use oneiric as filesystem on my customer board.I use HDMI as displayer,system can boot well,but can not login in.

The following is my bootargs:

video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24  root=/dev/mmcblk0p1 rootwait rw

After system boot,only part of the login UI is displayed,as my attachment login.jpg. In login  box,I can type linaro,and the enter,after a while,the display goes to all black and back to login.jpg soon.

I think HDMI driver is OK,when I enter CTRL+ALT+F1,the command line intercface is well as show in cmd.jpg.

Who can tell me what to do next?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,528件の閲覧回数
thouswave
Contributor III

sorry,I forget the cmd.jpg,show as following.

cmd.jpg

0 件の賞賛
返信

2,528件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 千 浪

problem with reboot may be caused by improper custom board

DDR settings (calibration coefficients) and memory size

(if different than in i.MX6 Sabre board). You can try DDR memory tool,

update Uboot flash_header.S and rebuild image

https://community.freescale.com/docs/DOC-96412

Best regards

igor

0 件の賞賛
返信

2,528件の閲覧回数
thouswave
Contributor III

I am sorry the problem is not DDR, but the command line. I have worked it out, the correct command line is as following:

console=ttymxc1,115200 mem=2048M video=mxcfb1:dev=ldb,LDB-XGA,if=RGB24 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 root=/dev/mmcblk0p2 rootwait rw ldo_active=on;bootm

Then ubuntu system can work well, but I really don't know why "video=mxcfb1:dev=ldb,LDB-XGA,if=RGB24" should be added. As I known,dev=ldb indicates that target display is LVDS. Now, I just use HDMI, but in the future, on our real product, LVDS is the main displayer. So, how to set the command line if the target display is LVDS?

0 件の賞賛
返信