omxplayer play issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

omxplayer play issue

5,605 次查看
allen_kim1
Contributor I

Dear NXP

 

my customer has a problem that  omxplayer playing issue 

 

Enviroment :  I.MX6 Quad  , Android :5.1.1_2.1.0 GA

169793_169793.jpgfolder.jpg 

i insert upper image as album art to mp3 file 

but omxplayer can't play that mp3 file 

 

Test Way : 

1  : i delete album art image , omxplayer can play that mp3 file

2  : i insert the other image into mp3 ( album art ) , omxplayer can play mp3 file

3 :  i insert upper image into mp3 ( album art ) , but omxplayer cannot play mp3 file 

 

 

i wonder why some specific image file is can't play on omxplayer 

 

 

other mp3 is same situation 

upper image into album art                --> omxplayer can not play that mp3 file 

upper image remove from  album art --> omxplayer can play that mp3 file 

other image into album art                 --> omxplayer can play that mp3 file 

Original Attachment has been moved to: mp3tag_error.log.zip

标记 (3)
0 项奖励
回复
3 回复数

5,045 次查看
joanxie
NXP TechSupport
NXP TechSupport

could you reproduce this issue on the latest android version?

0 项奖励
回复

5,045 次查看
joanxie
NXP TechSupport
NXP TechSupport

could you help check your issue as below? then tell me the result, thanks.

1)Check whether this issue is observed with PC media player, For example:
-  KMPlayer (http://www.kmplayer.com/)
-  VLC (http://www.videolan.org/vlc/)”

2)Check whether the same issue is observed in other Android benchmark device such as Nexus 7.

3)Check whether the issue exists when using Android Native player by running the below command on Freescale reference board.
- setprop media.omxgm.enable-player 0

 

Then run the test again.

4)Please check the media information with KMPlayer(menu to check the property of the video stream) and then check the multimedia release document to see if the video format is supported or not

0 项奖励
回复

5,045 次查看
allen_kim1
Contributor I

Dear Joan

Thanks for reply

that problem is omxplayer has a bug 

i received patch file from FAE

problem is solved

Thanks BR

0 项奖励
回复