Query on SC16IS750IBS (RS232, RS485 Controller I²C, SPI, UART Interface)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Query on SC16IS750IBS (RS232, RS485 Controller I²C, SPI, UART Interface)

747 次查看
manumathew
Contributor I

We had a query on SC16IS750IBS.

 

We would like to know if the GPIO0 pin of this device defaults to an input on power up?

标签 (1)
0 项奖励
回复
1 回复

696 次查看
b36401
NXP Employee
NXP Employee

Yes. They are inputs on power up.

  

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复