not able to boot custom imx6ull board using eMMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

not able to boot custom imx6ull board using eMMC

5,283件の閲覧回数
pankajjoshi
Contributor I

Hi,

I have created custom u-boot using DCD changes, custom kernel [zImage] with changes for UTP and USB_MASS_STORAGE in defconfig. Able to build the yocto images with customized u-boot, zImage and DTB. Able to flash via serial downloader using mfgtool2. I see all the output such as u-boot and kernel logs correctly on debug uart, But i am not able to get the board booted via eMMC after flashing. I do not see anything on serial. Can anyone faced the same issue. 

b45499‌ - Can you please help ! Added logs after flashing. Also DDR calibration is done for my KINGSTON DDR3L - 4G using DDR stress tester tool. I do not know why it still does not boot from eMMC. I see all the partitions created successfully. 

Is this some problem with boot partition 

in u-boot ./include/configs/mx6ullevk.h, CONFIG_SYS_MMC_ENV_PART = 0, is this problem due to it.

Any help is highly appreciated  !

ラベル(6)
0 件の賞賛
返信
6 返答(返信)

4,044件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Pankaj

was ddr memory of custom board tested by ddr stress tool

i.MX6/7 DDR Stress Test Tool V2.80 

New images should be rebuilt with new calibration settings forund from ddr test

(put them in uboot/../mx6ullevk/imximage.cfg).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,044件の閲覧回数
pankajjoshi
Contributor I

Hi Igor,

I have used the DDR stress test only with relevant changes in NXP aid script. Below is the calibration result i had

MMDC registers updated from calibration

Write leveling calibration
MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x00000000
MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x000A000A

Read DQS Gating calibration
MPDGCTRL0 PHY0 (0x021b083c) = 0x41580154
MPDGCTRL1 PHY0 (0x021b0840) = 0x00000000

Read calibration
MPRDDLCTL PHY0 (0x021b0848) = 0x40402E32

Write calibration
MPWRDLCTL PHY0 (0x021b0850) = 0x40403C38

I changed according to above calibration coefficient.

Please find the flashing logs coming in the debug uart [logsfromflashing.txt]. I see the uboot and kernel and rootfs loaded correctly. I see the partitioning of the eMMC as well. Can there be a problem of boot partition not enabled? Also the imx6ull inc file used for stress testing is attached [imxull.inc]. I used the "mfgtool2-yocto-mx-evk-emmc.vbs" file present in  mfgtool2. From flash logs present in logsfromflashing.txt, it looks everything went well. But not still sure why it did not flash from eMMC on reboot. 

If you still suggest, i can run through the DDR stress tester again. 

Please help as i am struck in the last step of the complete exercise. 

0 件の賞賛
返信

4,044件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Pankaj

could you clarify what do you mean by:

" But not still sure why it did not flash from eMMC on reboot. "

So described problem relates to mfg tool programming ?

Best regards
igor

0 件の賞賛
返信

4,044件の閲覧回数
pankajjoshi
Contributor I

My bad, i meant to say, it is flashing properly via mfgtool2. I see correct logs as well. However it does not boot from eMMC.

0 件の賞賛
返信

4,044件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

so is there any boot log from eMMC ?

If not any log, connect jtag and check boot configuration reading SRC_SBMR1,2

registers, check emmc signals with oscilloscope during boot.

Best regards
igor

0 件の賞賛
返信

4,044件の閲覧回数
pankajjoshi
Contributor I

Hi Igor,

Can you please have a look on my boot logs.

U-Boot 2017.03-nxp/imx_v2017.03_4.9.11_1.0.0_ga+ga2fea67 (Apr 26 2018 - 10:33:31 +0530)

CPU: Freescale i.MX6ULL rev1.0 528 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 52C
Reset cause: POR
Model: Freescale i.MX6 ULL 14x14 EVK Board
Board: MX6ULL 14x14 EVK
DRAM: 512 MiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment

Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc1(part 0) is current device
Net: No ethernet found.
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Kernel image @ 0x80800000 [ 0x000000 - 0x6d5178 ]
## Loading init Ramdisk from Legacy Image at 83800000 ...
Image Name: fsl-image-mfgtool-initramfs-imx6
Image Type: ARM Linux RAMDisk Image (gzip compressed)
Data Size: 8591032 Bytes = 8.2 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300bda2
Modify /soc/aips-bus@02200000/epdc@0228c000:status disabled
ft_system_setup for mx6

Starting kernel ...

Booting Linux on physical CPU 0x0
Linux version 4.9.11-1.0.0+gc27010d (lem@LEM) (gcc version 6.2.0 (GCC) ) #1 SMP PREEMPT Thu Apr 26 15:33:25 IST 2018
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d
CPU: div instructions available: patching division code
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt:Machine model: Freescale i.MX6 ULL 14x14 EVK Board
Reserved memory: created CMA memory pool at 0x8c000000, size 320 MiB
OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
Memory policy: Data cache writealloc
percpu: Embedded 14 pages/cpu @8bb31000 s25868 r8192 d23284 u57344
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= clk_ignore_unused
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 167548K/524288K available (9216K kernel code, 485K rwdata, 3236K rodata, 1024K init, 472K bss, 29060K reserved, 327680K cma-reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xa0800000 - 0xff800000 (1520 MB)
lowmem : 0x80000000 - 0xa0000000 ( 512 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80a00000 (10208 kB)
.init : 0x80e00000 - 0x80f00000 (1024 kB)
.data : 0x80f00000 - 0x80f796a0 ( 486 kB)
.bss : 0x80f7b000 - 0x80ff10e0 ( 473 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
Build-time adjustment of leaf fanout to 32.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80100000 - 0x80100058
Brought up 1 CPUs
SMP: Total of 1 processors activated (6.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor menu
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
imx6ul-pinctrl 2290000.iomuxc-snvs: initialized IMX pinctrl driver
mxs-dma 1804000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA, using PIO instead.
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA, using PIO instead.
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
PTP clock support registered
MIPI CSI2 driver module loaded
imx rpmsg driver is registered.
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.22
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
clocksource: Switched to clocksource mxc_timer1
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 8392K (83800000 - 84032000)
Bus freq driver module loaded
futex hash table entries: 256 (order: 2, 16384 bytes)
workingset: timestamp_bits=30 max_order=17 bucket_order=0
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.26)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
21c8000.lcdif supply lcd not found, using dummy regulator
mxsfb 21c8000.lcdif: failed to find mxc display driver
Console: switching to colour frame buffer device 60x34
mxsfb 21c8000.lcdif: initialized
imx-sdma 20ec000.sdma: loaded firmware 3.3
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 18, base_baud = 5000000) is a IMX
random: fast init done
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 73, base_baud = 5000000) is a IMX
imx-rng 2284000.rngb: iMX RNG Registered.
imx sema4 driver is registered.
[drm] Initialized
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
fsl-quadspi 21e0000.qspi: unrecognized JEDEC id bytes: ff, ff, ff
fsl-quadspi 21e0000.qspi: Freescale QuadSPI probe failed
fsl-quadspi: probe of 21e0000.qspi failed with error -2
spi_gpio spi4: gpio-miso property not found, switching to no-rx mode
libphy: Fixed MDIO Bus: probed
CAN device driver interface
flexcan 2090000.can: device registered (reg_base=a0a00000, irq=27)
flexcan 2094000.can: device registered (reg_base=a0a08000, irq=28)
20b4000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 20b4000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 20b4000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 1e:fb:1e:b2:c9:08
libphy: fec_enet_mii_bus: probed
fec 20b4000.ethernet eth0: registered PHC device 0
2188000.ethernet supply phy not found, using dummy regulator
pps pps1: new PPS source ptp1
fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: f2:a9:96:fd:c9:15
fec 2188000.ethernet eth1: registered PHC device 1
usbcore: registered new interface driver kaweth
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver
usbcore: registered new interface driver pegasus
usbcore: registered new interface driver rtl8150
usbcore: registered new interface driver r8152
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax88179_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb_ehset_test
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184000.usb supply vbus not found, using dummy regulator
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
LUN: removable read only file: /fat
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
mousedev: PS/2 mouse device common for all mice
input: 20cc000.snvs:snvs-powerkey as /devices/soc0/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0
input: iMX6UL Touchscreen Controller as /devices/soc0/soc/2000000.aips-bus/2040000.tsc/input/input1
read sensor who am i (0xfffffffa)error !
fxls8471: probe of 0-001e failed with error -22
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
pxp-v4l2 pxp_v4l2: initialized
0-000e supply vdd not found, using dummy regulator
0-000e supply vddio not found, using dummy regulator
mag3110 0-000e: check mag3110 chip ID
mag3110 0-000e: read chip ID 0xfffffffa is not equal to 0xc4!
mag3110: probe of 0-000e failed with error -22
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol BCSP registered
Bluetooth: HCI UART protocol ATH3K registered
usbcore: registered new interface driver bcm203x
usbcore: registered new interface driver btusb
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
wm8960 1-001a: Failed to issue reset
imx-wm8960 sound: failed to find codec platform device
imx-wm8960: probe of sound failed with error -22
NET: Registered protocol family 26
NET: Registered protocol family 10
mmc1: mmc_select_hs200 failed, error -74
mmc1: new MMC card at address 0001
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
NET: Registered protocol family 17
can: controller area network core (rev 20120528 abi 9)
mmcblk1: mmc1:0001 W62704 3.56 GiB
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20161123 t)
mmcblk1boot0: mmc1:0001 W62704 partition 1 2.00 MiB
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
mmcblk1boot1: mmc1:0001 W62704 partition 2 2.00 MiB
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
mmcblk1rpmb: mmc1:0001 W62704 partition 3 512 KiB
Bluetooth: BNEP filters: protocol multicast
Bluetooth: BNEP socket layer initialized
mmcblk1: p1 p2
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
cpu cpu0: Registered imx6q-cpufreq
imx_thermal 2000000.aips-bus:tempmon: Industrial CPU temperature grade - max:105C critical:100C passive:95C
dhd_module_init in
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
clk: Not disabling unused clocks
can-3v3: disabling
VSD_3V3: disabling
gpio_dvfs: disabling
ALSA device list:
No soundcards found.
Freeing unused kernel memory: 1024K (80e00000 - 80f00000)
Starting UTP
uuc 0.5 [built Sep 16 2016 02:36:28]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh mksdcard.sh /dev/mmcblk1'
UTP: executing "sh mksdcard.sh /dev/mmcblk1"
1+0 records in
1+0 records out
1024 bytes (1.0 kB, 1.0 KiB) copied, 0.095254 s, 10.8 kB/s
Checking that no-one is using this disk right now ... OK

Disk /dev/mmcblk1: 3.6 GiB, 38252 mmcblk1: p1 p2
05248 bytes, 7471104 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes

>>> Created a new DOS disklabel with disk identifier 0x459ca873.
Created a new partition 1 of type 'W95 FAT32 (LBA)' and of size 500 MiB.
/dev/mmcblk1p2: Created a new partition 2 of type 'Linux' and of size 3 GiB.
/dev/mmcblk1p3:
New situation:

Device Boot Start End Sectors Size Id Type
/dev/mmcblk1p1 20480 1044479 1024000 500M c W95 FAT32 (LBA)
/dev/mmcblk1p2 1228800 7471103 6242304 3G 83 Linux

The partition table has been altered.
Calling ioctl() to re-read partition table.
Syncing disks.
UTP: sending Success to kernel for command $ sh mksdcard.sh /dev/mmcblk1.
utp_poll: pass returned.
UTP: received command '$ dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=768 conv=fsync count=8'
UTP: executing "dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=768 conv=fsync count=8"
8+0 records in
8+0 records out
8192 bytes (8.2 kB, 8.0 KiB) copied, 0.0142733 s, 574 kB/s
UTP: sending Success to kernel for command $ dd if=/dev/zero of=/dev/mmcblk1 bs=1k seek=768 conv=fsync count=8.
utp_poll: pass returned.
UTP: received command '$ echo 0 > /sys/block/mmcblk1boot0/force_ro'
UTP: executing "echo 0 > /sys/block/mmcblk1boot0/force_ro"
UTP: sending Success to kernel for command $ echo 0 > /sys/block/mmcblk1boot0/force_ro.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2'
UTP: executing "dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2"
822+0 records in
822+0 records out
420864 bytes (421 kB, 411 KiB) copied, 0.208972 s, 2.0 MB/s
UTP: sending Success to kernel for command $ dd if=$FILE of=/dev/mmcblk1boot0 bs=512 seek=2.
utp_poll: pass returned.
UTP: received command '$ echo 1 > /sys/block/mmcblk1boot0/force_ro'
UTP: executing "echo 1 > /sys/block/mmcblk1boot0/force_ro"
UTP: sending Success to kernel for command $ echo 1 > /sys/block/mmcblk1boot0/force_ro.
utp_poll: pass returned.
UTP: received command '$ mmc bootpart enable 1 1 /dev/mmcblk1'
UTP: executing "mmc bootpart enable 1 1 /dev/mmcblk1"
UTP: sending Success to kernel for command $ mmc bootpart enable 1 1 /dev/mmcblk1.
utp_poll: pass returned.
UTP: received command '$ while [ ! -e /dev/mmcblk1p1 ]; do sleep 1; echo "waiting..."; done '
UTP: executing "while [ ! -e /dev/mmcblk1p1 ]; do sleep 1; echo "waiting..."; done "
UTP: sending Success to kernel for command $ while [ ! -e /dev/mmcblk1p1 ]; do sleep 1; echo "waiting..."; done .
utp_poll: pass returned.
UTP: received command '$ mkfs.vfat /dev/mmcblk1p1'
UTP: executing "mkfs.vfat /dev/mmcblk1p1"
mkfs.fat 3.0.28 (2015-05-16)
UTP: sending Success to kernel for command $ mkfs.vfat /dev/mmcblk1p1.
utp_poll: pass returned.
UTP: received command '$ mkdir -p /mnt/mmcblk1p1'
UTP: executing "mkdir -p /mnt/mmcblk1p1"
UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk1p1.
utp_poll: pass returned.
UTP: received command '$ mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1'
UTP: executing "mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1"
UTP: sending Success to kernel for command $ mount -t vfat /dev/mmcblk1p1 /mnt/mmcblk1p1.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ cp $FILE /mnt/mmcblk1p1/zImage'
UTP: executing "cp $FILE /mnt/mmcblk1p1/zImage"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/zImage.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ cp $FILE /mnt/mmcblk1p1/imx6ull-14x14-evk.dtb'
UTP: executing "cp $FILE /mnt/mmcblk1p1/imx6ull-14x14-evk.dtb"
UTP: sending Success to kernel for command $ cp $FILE /mnt/mmcblk1p1/imx6ull-14x14-evk.dtb.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext3 -F -E nodiscard /dev/mmcblk1p2'
UTP: executing "mkfs.ext3 -F -E nodiscard /dev/mmcblk1p2"
mke2fs 1.43-WIP (18-May-2015)
/dev/mmcblk1p2 contains a ext3 file system
last mounted on /mnt/mmcblk1p2 on Thu Jan 1 00:00:17 1970
Creating filesystem with 780288 4k blocks and 195072 inodes
Filesystem UUID: 93b59973-2012-44a5-b405-8f3c5ee5a11f
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912

Allocating group tables: done
Writing inode tables: done
Creating journal (16384 blocks): done
Writing superblocks and filesystem accounting information: done

UTP: sending Success to kernel for command $ mkfs.ext3 -F -E nodiscard /dev/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ mkdir -p /mnt/mmcblk1p2'
UTP: executing "mkdir -p /mnt/mmcblk1p2"
UTP: sending Success to kernel for command $ mkdir -p /mnt/mmcblk1p2.
utp_poll: pass returned.
UTP: received command '$ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2'
UTP: executing "mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2"
EXT4-fs (mmcblk1p2): mounting ext3 file system using the ext4 subsystem
EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
UTP: sending Success to kernel for command $ mount -t ext3 /dev/mmcblk1p2 /mnt/mmcblk1p2.
utp_poll: pass returned.
UTP: received command 'pipe tar -jxv -C /mnt/mmcblk1p2'
pid is 152, UTP: executing "tar -jxv -C /mnt/mmcblk1p2"
UTP: sending Success to kernel for command pipe tar -jxv -C /mnt/mmcblk1p2.

0 件の賞賛
返信