no operation audio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

no operation audio

1,381 次查看
kimsangyoung
Contributor I

Dear all

We use a new board was produced i.mx6q cpu . Please refer to the following log files. I do not know why the log file does not proceed further. However, the camera and movie works well . But the sound is not the behavior . The audio chip is used wm8962. movie play audio interface signal when the output does not come from i.mx6q .

Please tell me why why.

DACDAT: DAC data input

LRCLK: Left / Right data alignment clock

BCLK: Bit clock, for synchronisation

?

U-Boot 2009.08 (12??24 2014 - 15:15:41)

CPU: Freescale i.MX6 family TO1.2 at 792 MHz

Thermal sensor with ratio = 180

Temperature: 16 C, calibration data 0x5764c77d

mx6q pll1: 792MHz

mx6q pll2: 528MHz

mx6q pll3: 480MHz

mx6q pll8: 50MHz

ipg clock : 66000000Hz

ipg per clock : 66000000Hz

uart clock : 80000000Hz

cspi clock : 60000000Hz

ahb clock : 132000000Hz

axi clock : 264000000Hz

emi_slow clock: 132000000Hz

ddr clock : 528000000Hz

usdhc1 clock : 198000000Hz

usdhc2 clock : 198000000Hz

usdhc3 clock : 198000000Hz

usdhc4 clock : 198000000Hz

nfc clock : 24000000Hz

Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]

Boot Device: MMC

I2C:   ready

DRAM:   1 GB

MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3

*** Warning - bad CRC or MMC, using default environment

In: serial

Out: serial

Err: serial

Found PFUZE100! deviceid=10,revid=11

Net:   got MAC address from IIM: 00:00:00:00:00:00

FEC0 [PRIME]

Hit any key to stop autoboot:  0

kernel   @ 10808000 (4841212)

ramdisk  @ 11800000 (496509)

kernel cmdline:

           use boot.img command line:

           console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale androidboot.serialno=2220b9d4dbc84cc9

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

Initializing cgroup subsys cpu

Linux version 3.0.35-06522-g0a3529b (root@dwlee-All-Series) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #2 SMP PREEMPT Tue Dec 30 12:02:42 KST 2014

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board

Ignoring unrecognised tag 0x54410008

Memory policy: ECC disabled, Data cache writealloc

CPU identified as i.MX6Q, silicon rev 1.2

PERCPU: Embedded 7 pages/cpu @c133e000 s6528 r8192 d13952 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 208128

Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x27b00000 vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale androidboot.serialno=2220b9d4dbc84cc9

PID hash table entries: 2048 (order: 1, 8192 bytes)

Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

Memory: 379MB 378MB 64MB = 821MB total

Memory: 819988k/819988k available, 228588k reserved, 441344K highmem

Virtual kernel memory layout:

vector  : 0xffff0000 - 0xffff1000   (   4 kB)

fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xfbe00000 - 0xffe00000   (  64 MB)

    vmalloc : 0xd9800000 - 0xf2000000   ( 392 MB)

lowmem  : 0xc0000000 - 0xd9000000   ( 400 MB)

pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .init : 0xc0008000 - 0xc0047000   ( 252 kB)

      .text : 0xc0047000 - 0xc0910548   (8998 kB)

      .data : 0xc0912000 - 0xc09ac438   ( 618 kB)

       .bss : 0xc09ac45c - 0xc0b34f7c   (1571 kB)

Preemptible hierarchical RCU implementation.

NR_IRQS:624

MXC GPIO hardware

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

arm_max_freq=1GHz

MXC_Early serial console at MMIO 0x2020000 (options '115200')

bootconsole [ttymxc0] enabled

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Security Framework initialized

SELinux: Initializing.

Mount-cache hash table entries: 512

Initializing cgroup subsys debug

Initializing cgroup subsys cpuacct

Initializing cgroup subsys freezer

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

CPU1: Booted secondary processor

CPU2: Booted secondary processor

CPU3: Booted secondary processor

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

print_constraints: dummy:

NET: Registered protocol family 16

print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal

print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal

print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

UV<0>

标签 (1)
0 项奖励
回复
1 回复

1,322 次查看
igorpadykov
NXP Employee
NXP Employee

HI kim

I would suggest to check codec connections with SDK (wm8962.c)

audio test

i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6 series

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复