Hi Francisco
i.MX6SX is modified version of Solo, so as preliminary
answer one can look at Table 2-21. Recommended connections for
unused analog interfaces IMX6DQ6SDLHDG,
however it may be recomended to wait for Hardware Development Guide
for SoloX to be released. Note, this applicable only for analog
interfaces, digital power domains should be always powered.
One can run applications without DDR, running them from QSPI or
EIM directly (xip), or loading it to internal RAM (OCRAM).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------