no ipu interrupts sometimes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

no ipu interrupts sometimes

1,247件の閲覧回数
pravverma
Contributor III

Hi,

Our coustom board is based on i.mx53 & we are using linux 2.6.35.

We are using mxc_v4l2_overlay.out application to capture & display.

Everything works fine, but sometimes there is no data on display.

We found that when there is no data on display, there is no ipu interrupt generated.

In working/non-working case, the code flow is same & there is no error.

I am not sure why the ipu interrupt is not getting generated sometimes?

Please help us to understand the problem.

Thanks,

Praveen

ラベル(2)
0 件の賞賛
返信
1 返信

1,140件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi praveen,

If there is any issue, you should see some error/warning messages in your console, also make sure to enable the camera input modprobe mxc_v4l2_capture. I suggest to read Chapter 11 of you MX53 BSP documentation linux reference manual in order to check all options and usage of the ipu unit test codes.

Regards

0 件の賞賛
返信