nfsserver: NFS daemon support not enabled in kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nfsserver: NFS daemon support not enabled in kernel

3,144 Views
jacobojimenez
Contributor I

Hello,

I want to share the file system of my SABRE board with my PC using NFS. I compile the core-image-base image with the nfs-server feature and nfs-utils. When I try to start the nfs server from /etc/init.d/nfsserver  get the following message "NFS daemon support not enabled in kernel".

How can I get the daemon support enabled?

Thank you.

0 Kudos
Reply
2 Replies

2,421 Views
b36401
NXP Employee
NXP Employee

Please try "modprobe nfsd" command if NFS support is built as kernel module.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,420 Views
jacobojimenez
Contributor I

Thank you Victor,

I have already tried that and i get the error:

FATAL: Module nfsd not found.

Cheers!

Jacobo

0 Kudos
Reply