nfsserver: NFS daemon support not enabled in kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

nfsserver: NFS daemon support not enabled in kernel

3,187件の閲覧回数
jacobojimenez
Contributor I

Hello,

I want to share the file system of my SABRE board with my PC using NFS. I compile the core-image-base image with the nfs-server feature and nfs-utils. When I try to start the nfs server from /etc/init.d/nfsserver  get the following message "NFS daemon support not enabled in kernel".

How can I get the daemon support enabled?

Thank you.

0 件の賞賛
返信
2 返答(返信)

2,464件の閲覧回数
b36401
NXP Employee
NXP Employee

Please try "modprobe nfsd" command if NFS support is built as kernel module.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,463件の閲覧回数
jacobojimenez
Contributor I

Thank you Victor,

I have already tried that and i get the error:

FATAL: Module nfsd not found.

Cheers!

Jacobo

0 件の賞賛
返信