new display LVDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

new display LVDS

1,578件の閲覧回数
giorgiofantin
Contributor I

Hi to everybody,

  i coming crazy to add a new lvds to my embedded linux. I have an i.MX6 with kernel versoin 3.0.35 and FS ubuntu 12.02.

It works fine, but now i have to add a new lvds with a resolution as 640 x 480. Its clock frequency is about 25.18 with a maximum of 28.33. I added in ldc.c the new resolution, but with default valued i get a clock frequency of 38 MHz. Searching on google, i found to modifify clock.c file (arch/arm/mach-mx6/clock.c) and set

clk_set_parent(&ldb_di0_clk, &pll5_video_main_clk);

Defautl value is clk_set_parent(&ldb_di0_clk, &pll2_pfd_352M);

Chanching it, the clock frequency goes from 38kHz to 33, but not to 25.

Can anyone help me?

Thnaks

タグ(5)
0 件の賞賛
返信
1 返信

1,326件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Giorgio,

Just as reference I'm adding a link to the other LVDS Clock thread created since these are very similar:

https://community.freescale.com/thread/353830

Regards,

Gustavo

0 件の賞賛
返信