network deadlock in Linux kernel 4.9 (IPSEC)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

network deadlock in Linux kernel 4.9 (IPSEC)

2,104件の閲覧回数
wolfgang_muees
Contributor II

Hi,

I am using Linux kernel 4.9 on the i.MX6 series.

If using ethernet MAC and IPSEC (for VPN), sometimes the system goes into deadlock.

The problem is in xfrm_input.c, in the  xfrm_input() function.

This function is called for each incomming network packet, and also for each decrypted packet.

Both calls came from (different) soft irqs, and as the resources were protected with spin_lock(), there will be a deadlock if both calls came at the same time.

The solution is to convert all spinlock functions in  xfrm_input() to use spinlock_bh() funktions.

Look at this patch:

https://patchwork.ozlabs.org/project/netdev/patch/[email protected]/

regards

Wolfgang

ラベル(1)
0 件の賞賛
返信
1 返信

2,090件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello wolfgang,

You should try one of the latest BSP 5.4.47 or 5.9 since it has more stable network, and must include the ethernet bug patch.

 

Regards

 

0 件の賞賛
返信