nand flash factory programming using u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

nand flash factory programming using u-boot

1,772件の閲覧回数
pietercardoen
Contributor II

Dear

How do you need to program a nand flash using u-boot? I have created an ubifs image using Yocto. This image is loaded using the mfgtool to RAM. I now want to program the nand flash and I'm facing trouble. This is the way I do it:

> setenv mtdparts mtdparts= nand_flash:32m(kernel),32m(dtb),64m(root),-(data)

> setenv mtdids nand0=nand_flash

> nand erase.chip

> mdtparts

> ubi part root

> ubi create root

> ubi write 0x8380 0000 root 0x12A0000            

                          (0x83800000 => the ubifs image is loaded there and 0x12A0000 is the size of the image)

> bootz  ${loadaddr} - ${fdt_addr}

I get:

VFS: Cannot open root device "ubi0:root" or unknown-block(0,0): error -19
[ 1.423467] Please append a correct "root=" boot option; here are the available partitions:
[ 1.431983] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)

Is this a good way of working or is it preferred to use another method to progam my imx6ul device?

Best regards

Pieter

0 件の賞賛
返信
1 返信

1,407件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Pieter

one can try patch for U-Boot that integrates nxp kobs utility into U-Boot

[U-Boot] i.MX6 nand bootupdate, reworked - Patchwork 

nxp provides only mfg tools option for nand programming, use *.vbs

script for board with nand, like mfgtool2-yocto-mx-sabreauto-nand.vbs

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信