mxcfb in device tree

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mxcfb in device tree

Jump to solution
2,360 Views
lyashmik
Contributor II

I am trying to set up the display imx6q-sabresd and from other blog posts on nxp I see that people are adding mxcfb* to their device tree, like this for example:

mxcfb1:fb@0 {
compatible =  "fsl,mxc_sdc_fb" ;
disp_dev =  "lcd" ;
interface_pix_fmt =  "RGB565" ;
mode_str = "CLAA-WVGA";
default_bpp = < 16 >;
int_clk = < 0 >;
late_init = < 0 >;
status =  "okay" ;
};
I am on kernel 5.17 imx-linux and I get an error during the build saying that it cannot parse it. Could someone tell me what I am missing.
0 Kudos
Reply
1 Solution
2,340 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @lyashmik 

I hope you are doing well.

 

You can refer to the imx6qdl-sabresd.dtsi and imx6q-sabresd.dts. there are no changes from 5.10 to 6.6.

 

Best regards,

Salas.

 

 

View solution in original post

2 Replies
2,341 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @lyashmik 

I hope you are doing well.

 

You can refer to the imx6qdl-sabresd.dtsi and imx6q-sabresd.dts. there are no changes from 5.10 to 6.6.

 

Best regards,

Salas.

 

 

2,265 Views
lyashmik
Contributor II
The problem was that I was using mainline linux repository instead of linux-imx repository. Thanks.
0 Kudos
Reply