mxc_v4l2 architecture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mxc_v4l2 architecture

Jump to solution
1,882 Views
anjojohn
Contributor IV

HI All

i have been trying to develop a driver for ov5645 based on ov5640 driver. So far in BSP i see two drivers for OV5640. ov5640.c and ov5640_mipi.c . which one should i  use. My processor is imx6 Duallite. Also i am struggling to understand the v4l2 architecture in imx6. Could anyone please share me how we are using the mxc_v4l2 capture, any architecture diagrams will be fine.

Regards

Anjo

Labels (1)
0 Kudos
Reply
1 Solution
1,528 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anjo

please check Chapter 9 Video for Linux Two (V4L2) Driver

attached Linux Manual and presentation on

A Deep Dive into Image Processing for i.MX 6 Se... | NXP Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,529 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anjo

please check Chapter 9 Video for Linux Two (V4L2) Driver

attached Linux Manual and presentation on

A Deep Dive into Image Processing for i.MX 6 Se... | NXP Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------