mx8qmlpd4cpu which machine for yocto build

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mx8qmlpd4cpu which machine for yocto build

1,588 次查看
Salati
Contributor I

Hi,

try to build a sdcard image for a mx8qmlpd4cpu board with "Yocto Project User's Guide - Rev. L5.4.47_2.2.0"

I selected the imx8qmlpddr4arm2.conf file, is this correct?

bitbake image name --> fsl-image-machine-test

With the loaded .wic image to the sdcard, the board don't boot.

Do I need a .sdcard image? If so, how can I create one (with IMAGE_FSTYPES, but I saw it's no-more supported in"image_type.bbclass")?

0 项奖励
回复
2 回复数

1,570 次查看
Salati
Contributor I

Hi nxf63675,

Yes, it's a i.MX8 quad max with lpddr4. And the board boots with a very old .sdcard image but not with the new build

Thank you for the links, I tried as described in the manual but the board will not start.

My last attempt was to copy all files manually to the SD, as described in "Linux User Guide - 4.3.1 Preparing an SD/MMC card to boot" but with no success.

Why is there no more a .sdcard image?

What I can try, next?

0 项奖励
回复

1,576 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Hi Salati,

 

So for the machine file that you selected should be correct, just confirm, that the device that you are using is the i.MX8 quad max with LPDDR4, if yes, the file that you are using is the correct one.

 

And for boot from the SD card, Please be sure that you have the correct boot mode, you can check the reference manual to check this:

https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true

 

And if you need some clues of what to di next you can also check the next link:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8-Boot-process-and-creating-a-bootab...

 

Hope this helps you.

Regards,

Israel H.

0 项奖励
回复