mx8-dsi-oled1 touch not working with imx8mmevk board using yocto image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mx8-dsi-oled1 touch not working with imx8mmevk board using yocto image

跳至解决方案
2,116 次查看
Bharat
Contributor I

I have been working with the imx8mmevk board with  NXP MX8 DSI OLED1 screens attached, and I can't get the touch to work. I followed the instructions in the i.MX Yocto Project User's Guide, and I am able to build an image where the display is working, but touch is not. I am using imx8mm-evk-rm67191 for the device tree.

Is there a device tree for this board which does support the MX8 DSI OLED1 with touch?

If not, what all do I need to do to add touch support to imx8mm-evk-rm67191?

0 项奖励
回复
1 解答
2,075 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

After you change the kernel, you need also need to add it to weston, so you can try the steps here https://wiki.st.com/stm32mpu/wiki/How_to_calibrate_the_touchscreen.

You can tell us the test result.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,110 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

I do not know which version of BSP are you using, but you can refer to this :

https://source.codeaurora.org/external/imx/linux-imx/commit/?h=lf-5.10.y&id=57c43b67c169d91f4e4642b5...

0 项奖励
回复
2,089 次查看
Bharat
Contributor I

Thank you for your reply 

We are using yocto project with Distro-"fsl-imx-wayland" ,Distro_version "5.4-zeus" for imx8mmevk board with linux kernel version 5.4.70 .

As per your solution ,unfortunately imx8mp-evk-rm67199.dts/imx8mm-evk-rm67199.dts not available instead of that imx8mm-evk-rm67191.dts file is available.

I changed imx8mm-evk-rm67191.dts file as per imx8mp-evk-rm67199.dts provided by you but still not touch is not working .

Thank you.

 

0 项奖励
回复
2,076 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

After you change the kernel, you need also need to add it to weston, so you can try the steps here https://wiki.st.com/stm32mpu/wiki/How_to_calibrate_the_touchscreen.

You can tell us the test result.

0 项奖励
回复