mx6sx simple i2c write function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mx6sx simple i2c write function

1,198件の閲覧回数
dscott_ueidaq
Contributor I

I need to output a 16-bit value to a single i2c device at boot time. 

A simple polled write with no interrupts or dma is all I need.

This will be on a mx6sx using i2c4.

Is there an example that you could point me to?

0 件の賞賛
返信
1 返信

1,181件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @dscott_ueidaq 

I hope you are doing well.

You can use i2cset and i2cget Linux commands. Please find the reference from below.

To write the data: i2cset -y <I2C Bus No.> <Slave address> <Offset> <Data>

To read the data: i2cget -y <I2C Bus No.> <Slave address> <Offset>

Thanks & Regards

Sanket Parekh

0 件の賞賛
返信