mx6sl Custom Board. boot device configuration.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx6sl Custom Board. boot device configuration.

Jump to solution
2,870 Views
changyonglee
Contributor II

Hi. All.

want to boot i.MX6SoloLite Custom Board From eMMC Interface, for that I need to configure the boot device selection.(BT_FUSE_SEL or eFUSE)

How can Configure the BT_FUSE_SEL value or eFUSE value. ?

ver : uboot-2009.08, linux-3.0.35

Regards,

1 Solution
2,619 Views
igorpadykov
NXP Employee
NXP Employee

Hi changyong

please check

Q&A: How to program i.MX6 eFUSE?

https://community.freescale.com/docs/DOC-95458

~igor

View solution in original post

3 Replies
2,619 Views
igorpadykov
NXP Employee
NXP Employee

Hi changyong

please check sect.8.5.2.1 Expansion Device eFUSE Configuration

IMX6SLRM  i.MX 6SoloLite Applications Processor Reference Manual

and Chapter 7 Avoiding Board Bring-up Problems

IMX6SLHDG Hardware Development Guide for i.MX 6SoloLite - User Guide

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,619 Views
changyonglee
Contributor II

Hi. igorpadykov.

I want to know to write eFUSE on iMX6SL(BOOT_CFG)

Best regards.캡처.PNG

0 Kudos
Reply
2,620 Views
igorpadykov
NXP Employee
NXP Employee

Hi changyong

please check

Q&A: How to program i.MX6 eFUSE?

https://community.freescale.com/docs/DOC-95458

~igor