mx6s_csi_irq_handler Rx fifo overflow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx6s_csi_irq_handler Rx fifo overflow

5,859 Views
ngreen
Contributor II

Hi,

 

We (Yakov Shaulov and I) created custom board based on imx6slevk bsp and we connected parallel camera (gc0309 640x480 sensor) - created driver based on ov5640 located at subdev folder)

 

when we are trying to capture an image (using "gst-launch-1.0 v4l2src device=/dev/video0 num-buffers=1 ! jpegenc ! filesink location=capture.jpeg") most of the time we get "mx6s_csi_irq_handler Rx fifo overflow" and the image we get is corrupt

Original Attachment has been moved to: imx6sl_kernel_log.txt.zip

Labels (4)
4 Replies

5,007 Views
mulancc
Contributor I

i have same error ,  mx6s_csi_irq_handler Rx fifo overflow , imx6ul + ov9655,  but imx6ul + ov5640 ok

0 Kudos
Reply

5,004 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nadav

before using gstreamer please try some basic camera unit tests in

imx-test-..test/pxp_v4l2_test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

if it works then try gstreamer using sect.7.3.3 Video encoding

attached Linux Guide.

Please use nxp gstreamer plugins (fsl-gst-plugin) and official bsp releases described on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,004 Views
ngreen
Contributor II

Hi Igor

in section 7.3.3 (Video Encoding) it says that Video encoding requires VPU
we only need pictures captures and we don't have VPU (nor GPU on the board)

as I mentioned we are using "gst-launch-1.0 v4l2src device=/dev/video0 num-buffers=1 ! jpegenc ! filesink location=capture.jpeg" or using "gst-launch-1.0 imxv4l2src device=/dev/video0 num-buffers=1 ! jpegenc ! filesink location=capture.jpeg"

the error ("mx6s_csi_irq_handler Rx fifo overflow") appears often

(we are using a custom board based on i.MX6SL with GalaxyCore gc0309 VGA CMOS Image Sensor [the sensor driver is placed in /drivers/media/platform/mxc/subdev] and we enabled CONFG_VIDEO_MXC_CSI_CAMERA, CONFIG_VIDEO_MXC_PXP_V4L2 & CONFIG_VIDEO_V4L2_SUBDEV_API)

0 Kudos
Reply

5,003 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nadav

 please look

GStreamer i.MX6 Image Capture 

as there is no any specific for i.MX jpeg gstreamer implementation one can post

it on gstreamer mail list

GStreamer: Mailing Lists 

Best regards
igor

0 Kudos
Reply