mx6q reboot problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
13,256件の閲覧回数
mrleo
Contributor IV

In arch/arm/kernel/process.c, arm_machine_restart () function,

Void arm_machine_restart (char mode, const char *cmd)

{

/ * Flush the console to make sure all the relevant messages make it

* out to the console drivers

Arm_machine_flush_console ();

/ * Disable interrupts first * /

Local_irq_disable ();

Local_fiq_disable ();

/ *

* Tell the MM system that we are going to reboot

* we may need it to insert some 1:1 mappings so that

* soft boot works

*

Setup_mm_for_reboot (mode);

/ * Clean and * / invalidate caches

Flush_cache_all ();

/ * Turn off caching * /

Cpu_proc_fin ();

/ * Push out any further dirty data, and ensure cache is empty

Flush_cache_all ();

/ *

* Now call the architecture specific reboot code

*

Arch_reset (mode, CMD);

/ *

* Whoops the architecture was unable to reboot

* Tell the user!

*

Mdelay (1000);

Printk ("Reboot failed - System halted\n");

While (1);

}

On the command line, enter the reboot command, but system is not reboot.

# reboot

SysRq: Emergency Remount R/O

EXT4-fs (mmcblk0p4): re-mounted. Opts: (null)

EXT4-fs (mmcblk0p6): re-mounted. Opts: (null)

Emergency Remount complete

Imx2-wdt imx2-wdt.0: Device shutdown: Expect reboot!

Restarting system


Last printk which gets into Klog is before cpu_proc_fin () function,

cpu_proc_fin() is call /arch/arm/mm/proc-v7.S


ENTRY(cpu_v7_proc_fin)

  mrc p15, 0, r0, c1, c0, 0 @ ctrl register

  bic r0, r0, #0x1000 @ ...i............

  bic r0, r0, #0x0006 @ .............ca.

  mcr p15, 0, r0, c1, c0, 0 @ disable caches

  mov pc, lr

ENDPROC(cpu_v7_proc_fin)

Why hang before cpu_proc_fin () function?how to  solve this problem?

ラベル(4)
タグ(1)
1 解決策
7,433件の閲覧回数
mrleo
Contributor IV

sorry,uboot is add "ldo_active=on"

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
7,434件の閲覧回数
mrleo
Contributor IV

sorry,uboot is add "ldo_active=on"

0 件の賞賛
返信
7,433件の閲覧回数
mrleo
Contributor IV

Hi,all

Inl /arch/arm/mm/proc-v7.S cpu_proc_fin()

ENTRY(cpu_v7_proc_fin)

  mrc p15, 0, r0, c1, c0, 0 @ ctrl register

  bic r0, r0, #0x1000 @ ...i............

  bic r0, r0, #0x0006 @ .............ca.

  mcr p15, 0, r0, c1, c0, 0 @ disable caches

  mov pc, lr

ENDPROC(cpu_v7_proc_fin)

Comment out the following line of code will be ok

@ bic r0, r0, #0x0006 @ .............ca.

7,433件の閲覧回数
fatalfeel
Contributor V

Comment out the following line of code will be ok

@ bic r0, r0, #0x0006 @ .............ca.

////

I try and fail

0 件の賞賛
返信
7,433件の閲覧回数
jimlentz
Contributor I

I am seeing the same problem on MX6Q.

I don't understand WHY these lines need to be commented out, yes it fixes it -- but why?

Why isn't the Freescale  kernel repository reflect this change if it's needed?

I also don't understand the reference to the LDO being the reason. What does the LDO have to do with cache?

0 件の賞賛
返信
7,433件の閲覧回数
agherzan
Contributor II

Why this fix? Do we have an explanation on what is actually happening here? I encounter the same issue on a custom imx6q based platform.

0 件の賞賛
返信
7,433件の閲覧回数
mrleo
Contributor IV

Hi agherazn,

Maybe is ldo_bypass will cause this issue, if you in uboot add "ldo_enabled=on" it is ok. reboot is will ok for you!

0 件の賞賛
返信
7,433件の閲覧回数
raymondwang
Senior Contributor I

mx6q reboot implementation located at /arch/plat-mxc/system.c function arch_reset(char mode,const char* cmd).

Just look through arch_reset code, you can realize that mx6 reboot is achieved by watchdog output.

  On sabresd board, it use WDOG2 output to reset external PMIC. If your board does not reboot properly,you can

check your WDOG2 output pin config.

  On my board ,we use WDOG1 to reset external PMIC, so add extra code to support WDOG1 output is necessary.

  Hope these info can help you.

7,435件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 件の賞賛
返信
7,433件の閲覧回数
mrleo
Contributor IV

Thanks

0 件の賞賛
返信