mx6q quard preassembled uboot flashing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mx6q quard preassembled uboot flashing

4,002 次查看
LLlypukag3e2010
Contributor I

Hi everyone!

Can smb help?

i have a braded unit with ubuntu 13.04 onboard and EOL support from manufacter.

BoardID: MX6Q/SDL-SabreSD. 2GB Ram onboard,

inside is old 2013 uboot without "stop load" function. it flashed to spi separately. partition with uboot mount in system with rw support.

I'm going to flash it by this manual https://boundarydevices.com/programming-emmc-on-i-mx-platforms/ and try pre-compilied ubuntu 18.04

I found uart and connected to console

so here is question:

Is it possible to use pre-assembled uboot for this platform https://boundarydevices.com/wiki/bd-sl-imx6/ (from wiki boundarydevices)  instead of original? i think there are ohther boardid but hardware is identic

0 项奖励
回复
9 回复数

3,570 次查看
rwadraa7
Contributor I

Your blog is great, congratulations on your great work!

0 项奖励
回复

3,904 次查看
humansur
Contributor I
0 项奖励
回复

3,966 次查看
LLlypukag3e2010
Contributor I

it was not the best idea. got brick and waste time for repair. sabre light u-boot even not started on sabresd

0 项奖励
回复

3,942 次查看
igorpadykov
NXP Employee
NXP Employee

provided links were given to make decision: what actual board in hands - Sabre SD or Sabre Lite

(as uboot logs may be misleading). Based on that you can proceed with flashing proper image.

 

Best regards
igor

0 项奖励
回复

3,994 次查看
igorpadykov
NXP Employee
NXP Employee

Hi LLlypukag3e2010

 

one can try, however this manual is for https://boundarydevices.com/wiki/bd-sl-imx6/

board, not NXP "SabreSD", so in general there is chance that it will not work.

 

Best regards
igor

 

0 项奖励
回复

3,990 次查看
LLlypukag3e2010
Contributor I

Hello, Igor. can you try to explain differences between that platforms?

as i see from description - they are almost similiar. main diference -2gb ram in my "SABRESD" instead 1gb in "boundarydevice". oh, one more thing - it's call "SABRE Lite" formerly.

https://boundarydevices.com/sabre-lite-name-change-bd-sl-i-mx6-built-to-freescale-sabre-lite-design/

main reason of question - i couldn't found jtag pins on my board, so in case wrong u-boot device just will be brick. and recover will be possible only with tl866...(

anyway, i'll share result of my experiment.

0 项奖励
回复

3,916 次查看
mpandoayw
Contributor I

Your blog is simply amazing, congratulations on your great work! UPSers

0 项奖励
回复

3,956 次查看
mpandoayw
Contributor I

Thank you so much for sharing such a useful information. I will definitely share this with others. 

0 项奖励
回复

3,984 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复