mx6 Solo and/or DualLight with two cameras (parallel interface)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx6 Solo and/or DualLight with two cameras (parallel interface)

Jump to solution
2,539 Views
ilangoodman
Contributor I

Is it possible with either the i.mx6 Solo or Dual Light to connect two cameras using two separate parallel interfaces, and receive the two video streams simultaneously? In this application we are not using any display devices, we just want to get the images / video from both cameras into memory. It's not even entirely clear to me whether the Solo has two parallel interfaces, though it seems that the Dual Light definitely does..

Thanks,

ilan

Labels (4)
0 Kudos
Reply
1 Solution
1,996 Views
Yuri
NXP Employee
NXP Employee

Yes, this is possible. The second CSI port is mux-ed with EIM signals.

View solution in original post

0 Kudos
Reply
2 Replies
1,997 Views
Yuri
NXP Employee
NXP Employee

Yes, this is possible. The second CSI port is mux-ed with EIM signals.

0 Kudos
Reply
1,996 Views
ilangoodman
Contributor I

Thanks Yuri. We're making an adapter board to add the second parallel interface to the Boundary Devices SABRE Lite board so we can test this.

** FOLLOW UP **

We've now got two OV5642 (10 bit parallel interface) streaming video simultaneously on the SABRE Lite board with DualLite processor. Thanks for your help!

0 Kudos
Reply