mx53 wec7 csi example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx53 wec7 csi example

1,968 Views
alexeym
Contributor III

Hello there,

I'm trying to get OV3640 sensor working with mx53qsb based board.

I've got bsp from Adeneo and what I've done:

1. Setup iomux config in WINCE700\platform\iMX53_QSB\src\DRIVERS\IPUV3\CAMERA\bspcsi.cpp

2. Set env variable BSP_CAMERA1

I see that camera driver loaded and initialized, but next sample

DirectShow Sample Camera Application for WEC7 & WEC2013 - Download: DShowTest

doesn't work with message:

Builing the graph failed hr=0x1

RunCaptureGraph: Core components needed for RunCaptureGraph unavailable.

Later I found USB Camera in WEC7 can't show Video Render

After removing

[-HKEY_CLASSES_ROOT\Filter\{B87BEB7B-8D29-423f-AE4D-6582C10175AC}]

[-HKEY_CLASSES_ROOT\CLSID\{B87BEB7B-8D29-423f-AE4D-6582C10175AC}]

Sample starts to work, I see in debug that driver actually speak to camera over i2c and data starts to flow over CSI_D_ pads but all I see on screen is black rectange.

So why do I need to remove those keys to get basic samle working?

I've seen Camera Driver chapter in mx53smd windows embedded compact 7 reference manual, but mx53qsb bsp missing camera app test mentioned in mx53smd doc.

So where do I go next?

Labels (4)
Tags (4)
0 Kudos
Reply
1 Reply

1,672 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi alexeym,

There is an app in wince 6 bsp "CamApp" please see attached source, to port it to wince7 build it as a subproject and test it out.

Hope this helps

0 Kudos
Reply