mx53 opengl es2.0 lib

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mx53 opengl es2.0 lib

2,632件の閲覧回数
pensive
Contributor I

在linux 下mx53 能否支持opengl es2.0?在哪下载相关资料及库文件 ?

ラベル(3)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

2,451件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi peng

yes, opengl es2.0 is supported. Information can be found in

mx53_start_linux.pdf included in package below

L2.6.35_11_09_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation 11.09

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,451件の閲覧回数
pensive
Contributor I

按照文档解压amd-gpu-bin-mx51,得到lib,include,bin等文件 ,bin下测试程序打开失败,打印如下:

./2dblt_perf

*** glibc detected *** ./2dblt_perf: free(): invalid pointer: 0x2ad95380 ***

能否提供这些测试程序源码?

0 件の賞賛
返信

2,451件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi peng

no, sources not open.

Available only libs in binaries.

Best regards

chip

0 件の賞賛
返信