mx53 cspi clk source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mx53 cspi clk source

1,678件の閲覧回数
pensive
Contributor I

how to use Low-Frequency Reference Clock for cspi . CSPI_PERIODREG=0x8000 is not

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,612件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi peng

CSPI_PERIODREG is used for clock defining pause beteween data transfers.

CSPI data transfer clocks are defined using ECSPIx_CONREG dividers

and CCM ECSPI_CLK_ROOT, check Figure 18-2. CCM Clock Tree

i.MX53 Reference Manual (rev.2.1  6/2012)

http://www.freescale.com/files/32bit/doc/ref_manual/iMX53RM.pdf

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------