mx51 Android R10.4(using ADS7846) , touchscreen didn't work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mx51 Android R10.4(using ADS7846) , touchscreen didn't work

ソリューションへジャンプ
2,616件の閲覧回数
zhaozhao
Contributor III

Hi all

     We are using ads7846 on our custom mx51 board(without battery). What I modified is :

1) make sure the touchscreen name is ads7846, and change TARGET_TS_DEVICE := "mxc_ts" to TARGET_TS_DEVICE := "ads7846"  in the file device/fsl/imx5x/BoardConfigCommon.mk

2) with getevent, I got :

     # getevent
add device 1: /dev/input/event1
  name:     "mxc_power_key"
add device 2: /dev/input/event0
  name:     "mxckpd"
could not get driver version for /dev/input/mice, Not a typewriter
add device 3: /dev/input/event2
  name:     "ads7846"
could not get driver version for /dev/input/mouse0, Not a typewriter
/dev/input/event2: 0001 014a 000calib xc = 392, x = 6177, yc = 300, y = 6589
00001
/dev/input/event2: 0003 0000 00000188
/dev/input/event2: 0003 0001 0000012c
/dev/input/event2: 0003 0018 00003a2d
/dev/input/event2: 0000 0000 00000000
calib xc = 379, x = 6241, yc = 297, y = 6572
/dev/input/event2: 0003 0000 0000017b
/dev/input/event2: 0003 0001 00000129
/dev/input/event2: 0003 0018 00003a3c
/dev/input/event2: 0000 0000 00000000
calib xc = 388, x = 6198, yc = 299, y = 6583
/dev/input/event2: 0003 0000 00000184
/dev/input/event2: 0003 0001 0000012b
/dev/input/event2: 0003 0018 00003a32
/dev/input/event2: 0000 0000 00000000
/dev/input/event2: 0001 014a 00000000
/dev/input/event2: 0003 0018 00000000
/dev/input/event2: 0000 0000 00000000
/dev/input/event2: 0001 014a 000calib xc = 397, x = 6161, yc = 385, y = 7243
00001
/dev/input/event2: 0003 0000 0000018d
/dev/input/event2: 0003 0001 00000181
/dev/input/event2: 0003 0018 00003a32
/dev/input/event2: 0000 0000 00000000
/dev/input/event2: 0001 014a 00000000
/dev/input/event2: 0003 0018 00000000
/dev/input/event2: 0000 0000 00000000

3) I calibrated the touch screen, and got the points that seem right.

I can draw lines on the screen  when using tslib under Linux.

I cannot get the right action under android(there seems to be some actions, but not correct). here is part of the logcat information.

V/EventHub( 1969): /dev/input/evcalib xc = 381, x = 6233, yc = 338, y = 6878
ent2 got: t0=37, t1=644371, type=1, code=330, v=1
V/EventHub( 1969): iev.code=330 keyCode=0 flags=0x00000000 err=-19
D/InputReader( 1969): Input event: device=0x10002 type=0x1 scancode=330 keycode=0 value=1
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=651758, type=3, code=0, v=381
D/InputReader( 1969): Input event: device=0x10002 type=0x3 scancode=0 keycode=0 value=381
V/EventHub( 1969calib xc = 380, x = 6237, yc = 343, y = 6921
): /dev/input/event2 got: t0=37, t1=651951, type=3, code=1, v=338
D/InputReader( 1969): Input event: device=0x10002 type=0x3 scancode=1 keycode=1 value=338
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=652158, type=3, code=24, v=14910
D/InputReader( 1969): Input event: device=0x10002 type=0x3 scancode=24 keycode=24 value=14910
V/EventHub( 1calib xc = 378, x = 6249, yc = 344, y = 6928
969): /dev/input/event2 got: t0=37, t1=652369, type=0, code=0, v=0
D/InputReader( 1969): Input event: device=0x10002 type=0x0 scancode=0 keycode=0 value=0clicked
I/InputReader( 1969): Device reconfigured: id=0x10002, name=ads7846, display size is now 800x480
I/InputManager-Callbacks( 1969): No virtual keys found for device ads7846.
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=690437, type=3, code=0, v=380
D/InputReader( 1969): Input event: device=0x10002 type=0x3 scancode=0 keycode=0 value=380
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=690817, type=3, code=1, v=343
D/InputReader( 1969): Input event: device=0x10002 type=0x3 scancode=1 keycode=1 value=343
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=691053, type=3, code=24, v=14923
D/InputReader( 1969): Input event: device=0x10002 type=0x3 scancode=24 keycode=24 value=14923
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=691275, type=0, code=0, v=0
D/InputReader( 1969): Input event: device=0x10002 type=0x0 scancode=0 keycode=0 value=0
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=724994, type=3, code=0, v=378
D/InputReader( 1969): Input event: device=0x10002 type=0x3 scancode=0 keycode=0 value=378
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=725253, type=3, code=1, v=344
D/InputReader( 1969): Input event: device=0x10002 type=0x3 scancode=1 keycode=1 value=344
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=725468, type=3, code=24, v=14927
D/InputReader( 1969): Input event: device=0x10002 type=0x3 scancode=24 keycode=24 value=14927
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=725681, type=0, code=0, v=0
D/InputReader( 1969): Input event: device=0x10002 type=0x0 scancode=0 keycode=0 value=0
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=805270, type=1, code=330, v=0
V/EventHub( 1969): iev.code=330 keyCode=0 flags=0x00000000 err=-19
D/InputReader( 1969): Input event: device=0x10002 type=0x1 scancode=330 keycode=0 value=0
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=805283, type=3, code=24, v=0
D/InputReader( 1969): Input event: device=0x10002 type=0x3 scancode=24 keycode=24 value=0
V/EventHub( 1969): /dev/input/event2 got: t0=37, t1=805291, type=0, code=0, v=0
D/InputReader( 1969): Input event: device=0x10002 type=0x0 scancode=0 keycode=0 value=0

Can anyone help me on this?

Thanks

ラベル(2)
0 件の賞賛
返信
1 解決策
1,984件の閲覧回数
zhaozhao
Contributor III

I solved this.

In the file  frameworks/base/libs/ui/InputReader.cpp, I made these changes:

void TouchInputMapper::dispatchTouch(nsecs_t when, uint32_t policyFlags,
        TouchData* touch, BitSet32 idBits, uint32_t changedId, uint32_t pointerCount,
        int32_t motionEventAction)

LOGD("in.x is %d, in.y is %d\n", in.x, in.y);
            // X and Y
            float x = float(in.x - mLocked.xOrigin - mRawAxes.x.getRange()*a) * mLocked.xScale / (1-2*a);
            float y = float(in.y - mLocked.yOrigin- mRawAxes.y.getRange()*a) * mLocked.yScale / (1-2*a);
            LOGD("f.x is %f, f.y is %f\n", x, y);

I found that the mLocked.xScale is 4095, which is supposed to be 800( The LCD is 800x480).

I modified the ads7846 related file in the kernel source code.

Make sure that the x_max is 800 and the y_max is 480 in the file arch/arm/mach-mx5/mx51_babbage.c

static struct ads7846_platform_data ads_info = {
#if 1
    .x_max          = 800,
    .y_max          = 480,
    .x_plate_ohms       = 180,
    .pressure_max       = 15000,
    .debounce_max       = 5,
    .debounce_tol       = 4,
    .debounce_rep       = 1,
    .get_pendown_state  = ads7843_pendown_state,
    .keep_vref_on       = 1,
    .settle_delay_usecs = 150,
    .wakeup             = true,

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,985件の閲覧回数
zhaozhao
Contributor III

I solved this.

In the file  frameworks/base/libs/ui/InputReader.cpp, I made these changes:

void TouchInputMapper::dispatchTouch(nsecs_t when, uint32_t policyFlags,
        TouchData* touch, BitSet32 idBits, uint32_t changedId, uint32_t pointerCount,
        int32_t motionEventAction)

LOGD("in.x is %d, in.y is %d\n", in.x, in.y);
            // X and Y
            float x = float(in.x - mLocked.xOrigin - mRawAxes.x.getRange()*a) * mLocked.xScale / (1-2*a);
            float y = float(in.y - mLocked.yOrigin- mRawAxes.y.getRange()*a) * mLocked.yScale / (1-2*a);
            LOGD("f.x is %f, f.y is %f\n", x, y);

I found that the mLocked.xScale is 4095, which is supposed to be 800( The LCD is 800x480).

I modified the ads7846 related file in the kernel source code.

Make sure that the x_max is 800 and the y_max is 480 in the file arch/arm/mach-mx5/mx51_babbage.c

static struct ads7846_platform_data ads_info = {
#if 1
    .x_max          = 800,
    .y_max          = 480,
    .x_plate_ohms       = 180,
    .pressure_max       = 15000,
    .debounce_max       = 5,
    .debounce_tol       = 4,
    .debounce_rep       = 1,
    .get_pendown_state  = ads7843_pendown_state,
    .keep_vref_on       = 1,
    .settle_delay_usecs = 150,
    .wakeup             = true,

0 件の賞賛
返信