mx27 ssi interface program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mx27 ssi interface program

ソリューションへジャンプ
1,987件の閲覧回数
zhangjay
Contributor II

Dear all

I am using imx27 cpu as your board processor, I want to use the ssi interface as i2s to control TW2835 chip which has audio codec inside, but I cannot find any sample codes to refer.

Is there any example I can refer to?

I can find the functions in ssi.c, but I don't know how to use them.

I want to use the ssi interface as i2s.

ラベル(3)
0 件の賞賛
返信
1 解決策
1,848件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

You need a codec driver for the TW2835. Could not find it under soc/codecs, so you would need to add support for this codec first.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,849件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

You need a codec driver for the TW2835. Could not find it under soc/codecs, so you would need to add support for this codec first.

0 件の賞賛
返信