mtd-utils-201006.tar.bz2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mtd-utils-201006.tar.bz2

ソリューションへジャンプ
3,747件の閲覧回数
qiaoweibiao
Contributor III

Processing: u-boot-tools

==========================

Processing: mtd-utils

=======================

Build path taken because: no prebuilt rpm,

Testing network connectivity

OK GPP:

Try mtd-utils-201006.tar.bz2.md5 from the GPP

http://bitshrine.org/gpp/mtd-utils-201006.tar.bz2.md5:

17:11:10 ERROR 404: Not Found.

Try mtd-utils-201006.tar.bz2 from the GPP

http://bitshrine.org/gpp/mtd-utils-201006.tar.bz2:

17:11:11 ERROR 404: Not Found.

Can't get: mtd-utils-201006.tar.bz2 at ./ltib line 802.

Died at ./ltib line 1392.

traceback:

main::build_host_rpms:1392

  main::host_checks:1447

   main:554

Started: Thu Jan 21 17:11:07 2016

Ended:   Thu Jan 21 17:11:11 2016

Elapsed: 4 seconds

These packages failed to build:

mtd-utils

Build Failed

who can help me to fix it ??

Thanks a lot.

ラベル(2)
1 解決策
3,317件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi hiao

below attached mtd-utils file, please put it to /opt/freescale/pkgs

directory.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
3,318件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi hiao

below attached mtd-utils file, please put it to /opt/freescale/pkgs

directory.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,317件の閲覧回数
qiaoweibiao
Contributor III

frist thanks for your right answer.

now i also need the

mtd-utils-201006-4K-218-224-support.patch

can you give me ?

thanks a lot .

for the log:

ocessing: u-boot-tools

==========================

Processing: mtd-utils

=======================

Build path taken because: no prebuilt rpm,

Testing network connectivity

OK GPP:

Try mtd-utils-201006-4K-218-224-support.patch.md5 from the GPP

http://bitshrine.org/gpp/mtd-utils-201006-4K-218-224-support.patch.md5:

18:41:55 ERROR 404: Not Found.

Try mtd-utils-201006-4K-218-224-support.patch from the GPP

http://bitshrine.org/gpp/mtd-utils-201006-4K-218-224-support.patch:

18:41:55 ERROR 404: Not Found.

Can't get: mtd-utils-201006-4K-218-224-support.patch at ./ltib line 802.

Died at ./ltib line 1392.

traceback:

main::build_host_rpms:1392

  main::host_checks:1447

   main:554

Started: Thu Jan 21 18:41:52 2016

Ended:   Thu Jan 21 18:41:55 2016

Elapsed: 3 seconds

These packages failed to build:

mtd-utils

Build Failed

0 件の賞賛
返信
3,317件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

please find file attached

~igor

3,317件の閲覧回数
qiaoweibiao
Contributor III

gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm

now i need this file ,

there is always 404 not find .

How can I  find thems by other means?

Thanks a lot .

0 件の賞賛
返信