mscale_ddr_tool_v210_setup.exe dont open

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mscale_ddr_tool_v210_setup.exe dont open

1,712 Views
851931531
Contributor I

I load the mscale_ddr_tool_v210_setup.exe for imx8m mini evk.  But I don't install it. my pc is windows10. pc

print "此应用无法在你的电脑上运行"。I also try to running in compatibility mode (Windows xp),but not successfully.so what can I do?

Labels (1)
0 Kudos
Reply
1 Reply

1,580 Views
igorpadykov
NXP Employee
NXP Employee

Hi 魏伟 魏

one can check sect.2.2 System Requirements MSCALE_DDR_Tool_User_Guide.pdf

included in ddr test package onhttps://community.nxp.com/docs/DOC-340179 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply