mmc0: Timeout waiting for hardware interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mmc0: Timeout waiting for hardware interrupt

3,388 Views
vineethhegde
Contributor II

Hai...

I am using i.MX6Q based board. Schematics is similar to the Sabre SD board. i got a error message as shown below.

>>> mmc0: Timeout waiting for hardware interrupt

Please suggest a solution.

Labels (1)
0 Kudos
Reply
1 Reply

1,503 Views
igorpadykov
NXP Employee
NXP Employee

Hi vineeth113

seems sd port is not working correctly. Since you are using customizing BSP,

recommended to test board with Freescale BSP or with SDK. Also check signals

with oscilloscope, connecting to port sd card.

Best regards

igor

0 Kudos
Reply