mmc error while reset and reboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mmc error while reset and reboot

ソリューションへジャンプ
8,172件の閲覧回数
yashavanthashet
Contributor V

Hi,

We are using i.MX8M custom board with Linux4.9.51_ga release.

We are facing mmc error after giving 'reset' command in uboot or  'reboot' command in kernel.

Please see the print below.

--------------------------------------------------------------------------------------

iWave-G27 >
iWave-G27 > reset
resetting ...

U-Boot SPL 2017.03-imx_v2017.03_4.9.51_imx8m_ga+g2537522 (Nov 09 2018 - 11:00:20)
PMIC:  PFUZE100 ID=0x10
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
Training FAILED
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
Training FAILED
Normal Boot
Trying to boot from MMC1
mmc_load_image_raw_sector: mmc block read error
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

---------------------------------------------------------------------------------------------

Anyone faced this issue?

Thanks in advance,

Regards,

Yashavantha

0 件の賞賛
返信
1 解決策
7,351件の閲覧回数
yashavanthashet
Contributor V

hi,

Since watchdog was not properly implemented in both hardware and software, the above issue had occurred.

Issue solved after proper watchdog implementation.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
7,351件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yashavantha

one can check if custom board shortly remove power from board in reboot as it is done on i.MX8M EVK with

nWDOG (pad GPIO1_IO02), U704 UM805RE  p.10 SPF-29615 MX8M EVK schematic,
PMIC_ON_REQ and produced in the same manner as Reset Button SYS_nRST SW1702 switch.

Schematics (1)
Design Files for the i.MX 8M Evaluation Kit (EVK)(REV 0)
https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/evaluatio...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

7,350件の閲覧回数
yashavanthashet
Contributor V

Hi Igor,

Thank you for your reply.

This looks hardware watchdog power recycle implementation. Why it is necessary?
Can SW reboot/reset alone won't work in i.MX8M?

Regards,
Yashavantha

0 件の賞賛
返信
7,351件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yashavantha

power recycle implementation avoids having to determine if a component critical

to rebooting the processor is in the necessary state to support a reboot.

Components that fit this category include (but may not be limited to):

    eMMC memory card (if the hardware RST_B pin is not connected.
    SD Card/socket (if the reset pin is not used to remove power to the SD Card)
    QSPI
    NOR
    LPDDR2/3 memory

So you should analyze and determine what causes failure.

Best regards
igor

0 件の賞賛
返信
7,352件の閲覧回数
yashavanthashet
Contributor V

hi,

Since watchdog was not properly implemented in both hardware and software, the above issue had occurred.

Issue solved after proper watchdog implementation.

0 件の賞賛
返信