Processor pins pull-up configuration resistor value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor pins pull-up configuration resistor value

ソリューションへジャンプ
3,431件の閲覧回数
nirmalluhana
Contributor IV

Hi,

Release: Yocto-Morty (4.9.51_GA)

Board: i.MX8MQ EVK

I want to configure processors pins as pull-up enabled from dts file but as I am gone through the TRM it indicates the bits for pull-up enabled/disabled.

So, if I set that bits then by which resistor value it is going to be used for pull-up enable?

Or there are any other values of registers available for that purpose?

Best regards,

Nirmal

ラベル(1)
1 解決策
3,140件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Nimal,

I confirmed that there is an internal 90K Ohm pull down RES on the IOs to avoid excessive current through the resistive voltage divider of input receiver, and to avoid receiver devices overstress at 2.5/3.3V voltage range. There is no control bit for pull down enable/disable. The pull down is described as “always on 90k pd res”

There is a Pull Up Enable (PUE on the GPIO registers) but it only controls the internal 27K Ohm pull up RES enable/disable.

Regards,

元の投稿で解決策を見る

4 返答(返信)
3,140件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Nirmal,


My apologies for the delay. The Pull Up / Pull Down for each pin is set to a specific value so it can be enabled or disabled but the value is fixed.


On the i.MX8M Reference Manual you can see each pad’s PUE (Pull Up Enable) bit on the register. The value of the pull up resistor is not shown here but you can see if on the Reset condition field on the i.MX8M datasheet. (link below)
https://www.nxp.com/docs/en/data-sheet/IMX8MDQLQCEC.pdf


However, there seems to be a mismatch as some pins show Pull Down instead of Pull Up which is referred to on their registers.


I’ll escalate this, so it gets addressed.
Regards,

0 件の賞賛
返信
3,140件の閲覧回数
nirmalluhana
Contributor IV

Hi,

 

Any update on this?

 

Best regards,

Nirmal

0 件の賞賛
返信
3,141件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Nimal,

I confirmed that there is an internal 90K Ohm pull down RES on the IOs to avoid excessive current through the resistive voltage divider of input receiver, and to avoid receiver devices overstress at 2.5/3.3V voltage range. There is no control bit for pull down enable/disable. The pull down is described as “always on 90k pd res”

There is a Pull Up Enable (PUE on the GPIO registers) but it only controls the internal 27K Ohm pull up RES enable/disable.

Regards,

3,140件の閲覧回数
nirmalluhana
Contributor IV

Thanks gusarambula,

Appreciate your support.

 

Regards,

Nirmal

0 件の賞賛
返信