mipi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mipi

5,466件の閲覧回数
sumosumo
Contributor I

hi

i am using imx6q on nitrogen6x. i am trying to operate my MIPI ov5640 cam but unfortunately without any success.

the camera / sensor doesn’t give out data ( and than i get time-out error )

streaming task paused, reason error (-5)

Execution ended after 9996617334 ns.

regards

0 件の賞賛
返信
8 返答(返信)

5,357件の閲覧回数
saurabh206
Senior Contributor III

Hi

Sumo

Which BSP are you using?

Can you verify your driver is loaded or not?

Thanks

Saurabh

0 件の賞賛
返信

5,357件の閲覧回数
sumosumo
Contributor I

hi

yes the driver is probed properly.

what do you mean by saying bsp?

thanks for the quick reply

regards

0 件の賞賛
返信

5,357件の閲覧回数
sumosumo
Contributor I

linux 3.10.17

0 件の賞賛
返信

5,357件の閲覧回数
saurabh206
Senior Contributor III

Hi,

Can you just confirm that OV5640 camera is enabled in your kernel configuration?

if OV5640 is configured as a module than you need to first modprobe it.

Thank

Saurabh

0 件の賞賛
返信

5,357件の閲覧回数
sumosumo
Contributor I

i run the modprobe command:

modprobe ov5640_camera_mipi

then i get:

mxc_v4l2_master_attach: 0

mxc_v4l2_master_attach: ipu1:/csi1 attached ov5640_mipi:mxc_v4l2_cap2

camera ov5640_mipi is found

lsmod:

ov5640_camera_mipi 52003  0
mxc_v4l2_capture   22921  2 ov5640_camera_mipi
ipu_bg_overlay_sdc  3931  1 mxc_v4l2_capture
ipu_still           1689  1 mxc_v4l2_capture
ipu_prp_enc         4607  1 mxc_v4l2_capture
ipu_csi_enc         2799  1 mxc_v4l2_capture
ipu_fg_overlay_sdc  4727  1 mxc_v4l2_capture
v4l2_int_device     1697  2 ov5640_camera_mipi,mxc_v4l2_capture

thanks again!

0 件の賞賛
返信

5,357件の閲覧回数
saurabh206
Senior Contributor III

Are you able to fixed issue?

0 件の賞賛
返信

5,357件の閲覧回数
sumosumo
Contributor I

no... still not working

any case it is driver's registers issue?

0 件の賞賛
返信

5,357件の閲覧回数
saurabh206
Senior Contributor III

Are you using Android or Linux rootfs?

0 件の賞賛
返信