micros-d to emmc - imx93

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

micros-d to emmc - imx93

583 次查看
michaelscott2371
Contributor I

Hey,

i saw on imx93 that only SD1 supports eMMC 5.1.

i want to connect another eMMC memory on my board that i want that the imx will be able to communicate with (will behave like an external extra memory). i don't want sd card

is it possible to convert the sd interface to eMMC interface somehow? if yes, any recommended IC?

 

thanks

0 项奖励
回复
1 回复

561 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

You could integrate an eMMC in another USDHC interface but would be limited to 4-bit bus width and also HS400 since there isn't another STROBE input, just in USDHC1 this is possible. This way you wouldn't use all the features of an eMMC and I would recommend to go with an SD.

JosephAtNXP_0-1734473832876.png

Regards

0 项奖励
回复