mfgtool error 1167

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mfgtool error 1167

1,123 次查看
littlejfet
Contributor I

Has anyone seen this error code reported before? While trying to program an imx233 using mfgtool I get this error and have no idea what it means. Here's the last few lines from the log file:


1 - Panel A Start processing Singlechip NAND <LIST/>.
1 - Panel A Start <CMD/> type="boot" body="Recovery" file="updater.sb" timeout="60" onError="" text="Booting update firmware.".
1 - Panel A DoBoot() - Failed to load C:\mfg\Profiles\BSP Firmware Updater\Linux Update\updater.sb to Recovery mode device. (err=1167)
1 - Panel A Finished <CMD/> type="boot" body="Recovery" file="updater.sb" timeout="60" onError="" text="Booting update firmware." FAIL code=1167.
Panel A: Updater Error 0x48f (1167) - The device is not connected.
2 - Panel A Finished processing Singlechip NAND <LIST/> : FAIL code=1167.

Thanks!

标记 (2)
0 项奖励
回复
0 回复数