mfgtool烧写工具os firmware下的u-boot-mx6q-sabresd.bin生成问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mfgtool烧写工具os firmware下的u-boot-mx6q-sabresd.bin生成问题

2,518 Views
wangyongkang
Contributor I

各位工程师好:

我们正在I.MX6D,android4.4.2上开发,现在硬件上想把1G内存升级到2G,请问mfgtool工具里/profile/MX6Q linux update /os firmware下的u-boot-mx6q-sabresd.bin这个文件是如何生成的?

Tags (2)
0 Kudos
Reply
1 Reply

2,270 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Dear wang yongkang,

Have you finished the u-boot porting by now? If yes, you can build and compile an OS Firmware for MFG. In the attachment I give you a document about the porting u-boot, it is on android 4.2. You can refer to it.


Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply