i.MX6DQ ERR005768 and boot device.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ ERR005768 and boot device.

Jump to solution
498 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ ERR005768.

I want to know the relationship between boot device and ERR005768.

I believe ERR005768 can occur when use NAND as boot device since secondary image is prepared generally when NAND is used.

How about other boot device?

ERR005768 can occur with other boot device? (e.g. eMMC, Parallel NOR, etc...)

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
1 Solution
396 Views
art
NXP Employee
NXP Employee

The ERR005768 silicon erratum is applicable to all boot modes that support redundant boot. These modes are:

-NAND Flash boot;

-SD/MMC/eMMC boot;

-SATA boot.


Have a great day,
Artur
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
397 Views
art
NXP Employee
NXP Employee

The ERR005768 silicon erratum is applicable to all boot modes that support redundant boot. These modes are:

-NAND Flash boot;

-SD/MMC/eMMC boot;

-SATA boot.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos