memtool reading IPU registers hangs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

memtool reading IPU registers hangs

2,394 Views
qufeiwang
Contributor I

on a custom board, the memtool reading IPU1 and IPU2 and VDOA modules hangs. Most other modules work fine.

[root@freescale home]# ./memtool IPU1.*
./memtool IPU1.*
SOC is mx6q

IPU1 Addr:0x2400000

I did enabled the all clocks as Yuri said, using the following lines:

./memtool 0x020c4068=0xffffffff

./memtool 0x020c406c=0xffffffff

./memtool 0x020c4070=0xffffffff

./memtool 0x020c4074=0xffffffff

./memtool 0x020c4078=0xffffffff

./memtool 0x020c407c=0xffffffff

./memtool 0x020c4080=0xffffffff

thanks a lot!

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,869 Views
igorpadykov
NXP Employee
NXP Employee

Hi Oufei

clock gating is described in sect.18.6.23 CCM Clock Gating Register 0 (CCM_CCGR0)

i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

what BSP are you using, please try

linux-2.6-imx.git - Freescale i.MX Linux Tree 

use imx-test (memtool)

www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.4.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,869 Views
qufeiwang
Contributor I

thanks igor,

I am using a file given by the chip distributor.

L3.0.35_4.1.0_130816_source

Looks like I need do a clean start from scratch.  I am new to IMX.

Is yocto the officially recommended ?

0 Kudos
Reply